UWB MAC Custom Session

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UWB MAC Custom Session

2,080 Views
tomzzzz
Contributor I

Prerequisites:
NCJ29D5 both ends now use AIO's SDK, and the functions and functions related to Customized Session have been enabled in the APP code, the low-power mode has been disabled, and nothing else has been modified.
Problematic:
1. Now the parameters configured by Responder RCM_RX_TIMEOUT configurable time in the NXP_UCI_CCC_Specification description can be configured from 50us-40000us, but now the configuration parameters cannot take effect from the current waveform, and the configuration is the same as 40000us and 20000us, resulting in the RX on time is too short.
Do other parameters need to be configured together to take effect?

2.The ranging can be started normally, but the ranging status code received on the initiator side is shown as follows
0x2: Transaction expired
The ranging status code received in Responder is shown below
0xF: Ranging Control Message lost (Not available for the controller)


The following is the configuration of the SET_APP_CONFIG_CMD parameters of the initiator

        UCI_SPI_DATA_TX_Buffer[0] = 0x21;
UCI_SPI_DATA_TX_Buffer[1] = 0x03;
UCI_SPI_DATA_TX_Buffer[2] = 0x00;
#if in_resp
        GPIO_PinWrite(GPIOC,2u,1u);
UCI_SPI_DATA_TX_Buffer[3] = 0x31;//0x24,0x21,0x28,0x2B
        
        UCI_SPI_DATA_TX_Buffer[4] = 0x03;
UCI_SPI_DATA_TX_Buffer[5] = 0x00;
UCI_SPI_DATA_TX_Buffer[6] = 0x00;
UCI_SPI_DATA_TX_Buffer[7] = 0x00;
UCI_SPI_DATA_TX_Buffer[8] = 0x0C;//0x0A,0x0B,0x09,0x08
        
UCI_SPI_DATA_TX_Buffer[9] = 0x04;//CHANNEL ID
UCI_SPI_DATA_TX_Buffer[10] = 0x01;
UCI_SPI_DATA_TX_Buffer[11] = 0x09;
        
        UCI_SPI_DATA_TX_Buffer[12] = 0x05;//ANCHORS
UCI_SPI_DATA_TX_Buffer[13] = 0x01;
UCI_SPI_DATA_TX_Buffer[14] = 0x01;
        
      UCI_SPI_DATA_TX_Buffer[15] = 0x08;//SLOT_LENGTH
UCI_SPI_DATA_TX_Buffer[16] = 0x02;
        UCI_SPI_DATA_TX_Buffer[17] = 0x60;//0x60,0x10,0xB0,0xC0
UCI_SPI_DATA_TX_Buffer[18] = 0x09;//0x09,0x0E,0x04,0x12
        
UCI_SPI_DATA_TX_Buffer[19] = 0x09;//RANGING_INTERVAL
        UCI_SPI_DATA_TX_Buffer[20] = 0x04;
UCI_SPI_DATA_TX_Buffer[21] = 0x18;//0x60,0x12,0x10,0x18,0x14
        UCI_SPI_DATA_TX_Buffer[22] = 0x00;
UCI_SPI_DATA_TX_Buffer[23] = 0x00;
UCI_SPI_DATA_TX_Buffer[24] = 0x00;
        
        UCI_SPI_DATA_TX_Buffer[25] = 0x11;//0x01 Device Role Initiator,0x00 Responder
UCI_SPI_DATA_TX_Buffer[26] = 0x01;
UCI_SPI_DATA_TX_Buffer[27] = 0x01;//0x00,0x01
 
        
        UCI_SPI_DATA_TX_Buffer[28] = 0xF2;//TX_POWER_ID
        UCI_SPI_DATA_TX_Buffer[29] = 0x01;
UCI_SPI_DATA_TX_Buffer[30] = 0x00;
 
        UCI_SPI_DATA_TX_Buffer[31] = 0x1B;//SLOTS_PER_RR
        UCI_SPI_DATA_TX_Buffer[32] = 0x01;
UCI_SPI_DATA_TX_Buffer[33] = 0x06; 
        
        UCI_SPI_DATA_TX_Buffer[34] = 0x02;//CUSTOM SESSION ONLY SUPPORT Static STS 0X00
        UCI_SPI_DATA_TX_Buffer[35] = 0x01;
UCI_SPI_DATA_TX_Buffer[36] = 0x00;
        
        UCI_SPI_DATA_TX_Buffer[37] = 0xE3;//RX_START_MARGIN
        UCI_SPI_DATA_TX_Buffer[38] = 0x01;
        UCI_SPI_DATA_TX_Buffer[39] = 0XFF;
        
        UCI_SPI_DATA_TX_Buffer[40] = 0xE4;//RX_TIMEOUT
        UCI_SPI_DATA_TX_Buffer[41] = 0x02;
        UCI_SPI_DATA_TX_Buffer[42] = 0xF4;
        UCI_SPI_DATA_TX_Buffer[43] = 0x01;
        
        UCI_SPI_DATA_TX_Buffer[44] = 0xFB;//RADIO_CFG_IDXS
        UCI_SPI_DATA_TX_Buffer[45] = 0x04;
        UCI_SPI_DATA_TX_Buffer[46] = 0x00;
        UCI_SPI_DATA_TX_Buffer[47] = 0x01;
        UCI_SPI_DATA_TX_Buffer[48] = 0x10;
        UCI_SPI_DATA_TX_Buffer[49] = 0x11;
        
        UCI_SPI_DATA_TX_Buffer[50] = 0x0C;
        UCI_SPI_DATA_TX_Buffer[51] = 0x01;
        UCI_SPI_DATA_TX_Buffer[52] = 0x03;
 
Below is the configuration of the SET_APP_CONFIG_CMD related parameters of Responder:
UCI_SPI_DATA_TX_Buffer[3] = 0x46;//0x24,0x21,0x28,0x2B
        
UCI_SPI_DATA_TX_Buffer[4] = 0x03;
UCI_SPI_DATA_TX_Buffer[5] = 0x00;
UCI_SPI_DATA_TX_Buffer[6] = 0x00;
UCI_SPI_DATA_TX_Buffer[7] = 0x00;
UCI_SPI_DATA_TX_Buffer[8] = 0x11;//0x0A,0x0B,0x09,0x08
        
UCI_SPI_DATA_TX_Buffer[9] = 0x04;//CHANNEL ID
UCI_SPI_DATA_TX_Buffer[10] = 0x01;
UCI_SPI_DATA_TX_Buffer[11] = 0x09;
        
 UCI_SPI_DATA_TX_Buffer[12] = 0x05;//ANCHORS
UCI_SPI_DATA_TX_Buffer[13] = 0x01;
UCI_SPI_DATA_TX_Buffer[14] = 0x01;
        
UCI_SPI_DATA_TX_Buffer[15] = 0x08;// SLOT_LENGTH
UCI_SPI_DATA_TX_Buffer[16] = 0x02;
UCI_SPI_DATA_TX_Buffer[17] = 0x60;//0x60,0x10,0xB0,0xC0
UCI_SPI_DATA_TX_Buffer[18] = 0x09;//0x09,0x0E,0x04,0x12
        
UCI_SPI_DATA_TX_Buffer[19] = 0x09;//RANGING_INTERVAL
UCI_SPI_DATA_TX_Buffer[20] = 0x04;
UCI_SPI_DATA_TX_Buffer[21] = 0x18;//0x60,0x12,0x10,0x18,0x14
UCI_SPI_DATA_TX_Buffer[22] = 0x00;
UCI_SPI_DATA_TX_Buffer[23] = 0x00;
UCI_SPI_DATA_TX_Buffer[24] = 0x00;
        
UCI_SPI_DATA_TX_Buffer[25] = 0x11;//0x01 Device Role Initiator,0x00 Responder
UCI_SPI_DATA_TX_Buffer[26] = 0x01;
UCI_SPI_DATA_TX_Buffer[27] = 0x00;//0x00,0x01
 
        
UCI_SPI_DATA_TX_Buffer[28] = 0xF2;//TX_POWER_ID
UCI_SPI_DATA_TX_Buffer[29] = 0x01;
UCI_SPI_DATA_TX_Buffer[30] = 0x00;
UCI_SPI_DATA_TX_Buffer[31] = 0x1B;//SLOTS_PER_RR
UCI_SPI_DATA_TX_Buffer[32] = 0x01;
UCI_SPI_DATA_TX_Buffer[33] = 0x06; 
        
UCI_SPI_DATA_TX_Buffer[34] = 0x02;//CUSTOM SESSION ONLY SUPPORT Static STS 0X00
UCI_SPI_DATA_TX_Buffer[35] = 0x01;
UCI_SPI_DATA_TX_Buffer[36] = 0x00;
 
 UCI_SPI_DATA_TX_Buffer[37] = 0x1E;//RESPONDER_SLOT_INDEX
 UCI_SPI_DATA_TX_Buffer[38] = 0x01;
UCI_SPI_DATA_TX_Buffer[39] = 0x00;
        
        UCI_SPI_DATA_TX_Buffer[40] = 0xEA;// RCM_RX_MARGIN_TIME
        UCI_SPI_DATA_TX_Buffer[41] = 0x03;
        UCI_SPI_DATA_TX_Buffer[42] = 0x01;
        UCI_SPI_DATA_TX_Buffer[43] = 0xE8;//0x40,0xE8,0x20
        UCI_SPI_DATA_TX_Buffer[44] = 0x03;//0x9C,0x03,0x4E
        
        UCI_SPI_DATA_TX_Buffer[45] = 0xEB;//RCM_RX_TIMEOUT
        UCI_SPI_DATA_TX_Buffer[46] = 0x03;
        UCI_SPI_DATA_TX_Buffer[47] = 0x01;
        UCI_SPI_DATA_TX_Buffer[48] = 0x40;//0x20
        UCI_SPI_DATA_TX_Buffer[49] = 0x9C;//0x4E
        
        UCI_SPI_DATA_TX_Buffer[50] = 0xE5;//ADAPTED_RANGING_INDEX (*)
        UCI_SPI_DATA_TX_Buffer[51] = 0x02;
        UCI_SPI_DATA_TX_Buffer[52] = 0xFF;
        UCI_SPI_DATA_TX_Buffer[53] = 0xFF;
        
        UCI_SPI_DATA_TX_Buffer[54] = 0xFB;//RADIO_CFG_IDXS
        UCI_SPI_DATA_TX_Buffer[55] = 0x04;
        UCI_SPI_DATA_TX_Buffer[56] = 0x00;
        UCI_SPI_DATA_TX_Buffer[57] = 0x01;
        UCI_SPI_DATA_TX_Buffer[58] = 0x10;
        UCI_SPI_DATA_TX_Buffer[59] = 0x11;
        
        UCI_SPI_DATA_TX_Buffer[60] = 0xE3;//RX_START_MARGIN
        UCI_SPI_DATA_TX_Buffer[61] = 0x01;
        UCI_SPI_DATA_TX_Buffer[62] = 0XFF;
          
        UCI_SPI_DATA_TX_Buffer[63] = 0xE4;//RX_TIMEOUT
        UCI_SPI_DATA_TX_Buffer[64] = 0x02;
        UCI_SPI_DATA_TX_Buffer[65] = 0xF4;
        UCI_SPI_DATA_TX_Buffer[66] = 0x01;
        
        UCI_SPI_DATA_TX_Buffer[67] = 0xF1;//RR_RETRY_THR
        UCI_SPI_DATA_TX_Buffer[68] = 0x02;
        UCI_SPI_DATA_TX_Buffer[69] = 0x00;
        UCI_SPI_DATA_TX_Buffer[70] = 0x64;
        
        UCI_SPI_DATA_TX_Buffer[71] = 0x0C;
        UCI_SPI_DATA_TX_Buffer[72] = 0x01;
        UCI_SPI_DATA_TX_Buffer[73] = 0x03;
Tags (1)
0 Kudos
Reply
1 Reply

2,057 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Sorry for the inconvenience this might cause you but as the information of these products it's under NDA (Non-Disclosure Agreement) the information it's not public, this is not a secure channel to share any information of this device and I do not have the data as well for the same reason.

 

For more information about the chips and buying process, could you please contact one of our distributors available in the Distributor Network|NXP? They can not only help you with the NDA process, but also help you check if you can get documentation and the information they can offer you.

 

Regards,

Ricardo

0 Kudos
Reply