UWB AT command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UWB AT command

2,482 Views
Arjun_Bansal
Contributor II

Hi guys

I have seen few documents related to UWB. They mention about AT commands are used for UWB.

I have got only few AT commands.

I really in need of these AT commands to start my development, please help me to provide AT command and other information necessary for development point of view.

0 Kudos
Reply
2 Replies

1,758 Views
clark598dahl
Contributor I

Hello @Arjun_Bansal,
I’m starting UWB development and need a full set of AT commands—currently have only a few. Can anyone share documentation or examples for configuring and running ranging sessions via AT commands?

Best Regards,
Clark Dahl

0 Kudos
Reply

2,462 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of these products it's under NDA (Non-Disclosure Agreement) the information it's not public.

In case you are looking for information about our UWB products or you are interested in this technology, I would recommend you check these Development Kits and Modules from our Partners (Trimension UWB Partners).

In case you are interested in one of these Kits/Modules, you would need to go directly with them to know the process and the support that they can provide them, as the support path for this technology is through them.

 

Regards,

Ricardo

0 Kudos
Reply