OL2385 - 868 MHz data rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OL2385 - 868 MHz data rate

2,356件の閲覧回数
JiaNa
NXP Employee
NXP Employee

Hi, I would like to know what is the maximum data rate for 868 MHz in OL2385. In OL2385 datasheet, it mentioned that the maximum data rate up to 400 kbit/s.

ラベル(2)
0 件の賞賛
返信
1 返信

2,340件の閲覧回数
prakashram72
Contributor III

Hi @JiaNa 

Yes, you are correct. According to the OL2385 datasheet, the maximum data rate for the 868 MHz frequency band is indeed up to 400 kbit/s. This is the maximum speed at which data can be transferred using this product under ideal conditions. However, please note that actual data rates can vary depending on a variety of factors, including the quality of the transmission medium, the distance between the transmitter and receiver, and the presence of any interference.

0 件の賞賛
返信