OL2385 - 868 MHz data rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OL2385 - 868 MHz data rate

2,346 次查看
JiaNa
NXP Employee
NXP Employee

Hi, I would like to know what is the maximum data rate for 868 MHz in OL2385. In OL2385 datasheet, it mentioned that the maximum data rate up to 400 kbit/s.

标签 (2)
0 项奖励
回复
1 回复

2,330 次查看
prakashram72
Contributor III

Hi @JiaNa 

Yes, you are correct. According to the OL2385 datasheet, the maximum data rate for the 868 MHz frequency band is indeed up to 400 kbit/s. This is the maximum speed at which data can be transferred using this product under ideal conditions. However, please note that actual data rates can vary depending on a variety of factors, including the quality of the transmission medium, the distance between the transmitter and receiver, and the presence of any interference.

0 项奖励
回复