LID2580 Usage Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LID2580 Usage Issues

2,033 Views
wanzhu
Contributor I

May I ask how to use the LID2580 board? Our company recently purchased a batch. I saw in the documentation that there are CAS, AIO, SR, and CCC—what do each of them represent? How should I quickly get it to work?

Labels (1)
0 Kudos
Reply
4 Replies

2,009 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Sorry for the inconvenience this might cause you but as the information of this product it's under NDA (Non-Disclosure Agreement) the information it's not public.

For more information about the chip could you please contact one of our distributors available in the Distributor Network|NXP? Or if you have any direct contact who helped you getting this device, please contact them.

If you are looking for information about our UWB products or you are interested in this technology, I would recommend you check these Development Kits and Modules from our Partners (Trimension UWB Partners).

In case you are interested in one of these Kits/Modules, you would need to go directly with them to know the process and the support that they can provide them, as the support path for this technology is through them.

The documentation and software are distributed by the corresponding UWB Module partner. By selecting a module, you will be guided to our partner’s page where you can access datasheets, application notes, and the required enablement

 

Regards,

Ricardo

0 Kudos
Reply

1,980 Views
wanzhu
Contributor I

Hello, our company has already signed an NDA with NXP. How can I find the corresponding materials? I just recently joined the company and don’t know which distributor the purchase was made from at that time, so I cannot find the LIO2580 user manual.

0 Kudos
Reply

1,965 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

You would need to go with the person that help you getting the board.

I apologize for the inconveniences.

 

Regards,

Ricardo

0 Kudos
Reply

1,935 Views
wanzhu
Contributor I

Hello, I had this problem when I downloaded the NCJ29D6 program in KEIL, and I didn't figure it out for a few days, can you help me see what's going on?

 

* JLink Info: Memory map 'after startup completion point' is active
***JLink Error: Could not start CPU core. (ErrorCode: -1)
***JLink Error: Cannot read register 15 (R15) while CPU is running
***JLink Error: Cannot read register 20 (CFBP) while CPU is running
***JLink Error: CPU is not halted
***JLink Error: Cannot read register 15 (R15) while CPU is running
Full Chip Erase Failed!
Flash Erase finished 13:28:01

0 Kudos
Reply