programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

programming

2,625件の閲覧回数
cy
Contributor I

I have completed the jm60 board open design. I have a MC9S08JM16CLC on board and am needing some insight on how to program the chip. I have at my disposal a usbsyder programmer or a HC912B eval board. Is there any good tutorial on how to programm the JM16 for the first time? Thanks for the help.

 

Cy

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,350件の閲覧回数
cy
Contributor I
The serial programming of a BDM interface is not something I fully understand, but any BDM driver can not program any BDM interfaced chip. Freescale's advice is either of two $500.00 programmers to get the job done. I was able to procure a P&E USB HCS08/HCS12 Multilink which worked fine loading the .s19 file through the Hiwave of the code warrior software. I had access to a USB mon08 ML 12 as well I am not sure but this may be able to get the job done as well with a bit of interface manipulation 16 pin to 6 pin.
0 件の賞賛
返信