osbdm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

osbdm

1,708件の閲覧回数
jawwaj
Contributor II

Hi, i had buy a DEVKIT-S12XE, which includes an osbdm debugger, but does not work with the NOICE.

DEVKIT-S12XE development platform for S12XE|NXP 

Iis it possible to change the OSBDM firmware to function as a USBDM?

0 件の賞賛
返信
1 返信

1,433件の閲覧回数
pgo
Senior Contributor V

Hi jaw waj,

I do not have access to this board for testing.

It appears to be a standard OSBDM-JM60 hardware so it may work with the USBDM_TWR_HCS12_V4.sx image provided in the USBDM installation FlashImages folder.

However - this requires programming the image to the board.  It is not in the format compatible with the OSBDM bootloader.  You will require an external HCS08 programmer.

bye

0 件の賞賛
返信