first steps- OSBDMJB16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

first steps- OSBDMJB16

2,533件の閲覧回数
novi
Contributor I

Hi all,

 

I need a some help. 

I am using USBDM JB16 -- http://www.wayengineer.com/index.php?main_page=product_info&products_id=289

 

USBDMJB16  not responding.

I purchased this debugger for an HCS08 based microcontroller project. I was planning on using an Windows XP SP2 system and CodeWarrior 6.3 for MCU ,BDM firmware v2.0 or v4.5

 

This is my first attempt to use HCS08 back ground debug my experience is with HC08.

Am I missing something?

does the flash program .s19 in the my new USBDM JB16 mikrokontroler ?

Any help would be appreciated.

Thank you

regards

ラベル(2)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,251件の閲覧回数
novi
Contributor I

ok,

 

 

Tnx

regards

0 件の賞賛
返信

2,251件の閲覧回数
novi
Contributor I

Mickey:

 

When I buy OSBDM with processor HC908JB16, is it empy and I have to firmware  or it has software?

How I can check it has firmware?

0 件の賞賛
返信

2,251件の閲覧回数
pgo
Senior Contributor V

Dear Novi,

 

The JB16 version of USBDM is really obsolete.

 

However, you can still try the current firmware etc with it.

 

I suggest you download the USBDM software and install it.  You will also need to update the firmware.

 

Documentation:

http://usbdm.sourceforge.net/

 

Software/Drivers/Firmware:

http://sourceforge.net/projects/usbdm/files/Version%204.9/

 

Good luck!

bye

0 件の賞賛
返信

2,251件の閲覧回数
Mickey
Contributor III

The first must go first, "http://www.wayengineer.com" If they do not have a good after-sales service, and that cheap is useless.

0 件の賞賛
返信