dll that provide an API for using the BDM interface??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dll that provide an API for using the BDM interface??

5,440 Views
Leo_A
Contributor I

Hi,

I am using a microcontroller of the HCS12 familly and I am wondering is if there is available a dynamic-link library (.dll) that provide an Applications Programming Interface (API) for using the Background Debuger Module(BDM) interface.

I already have a a cable to connect the PC via serial to the BDM port in the microcontroller, and I use it with the debugger that the codewarrior has, but what I need is that instead of using the debugger available in the codewarrior, integrate some of the debugger capabilities in a different program.

Regards, Leo



Message Edited by Leo_A on 2008-10-21 10:35 PM
0 Kudos
Reply
3 Replies

1,797 Views
Leo_A
Contributor I
pgo,
 
Yes, I am using a different cable, a USB BDM Multilink cable from P&E Micro.
 
Thanks for your response, I am going to try in the CW forum.
 
Regards, Leo_A
0 Kudos
Reply

1,797 Views
pgo
Senior Contributor V
Dear Leo_A,

P&E Micro have a development kit available that would be what you want (
)

Check their web site.

bye

0 Kudos
Reply

1,797 Views
pgo
Senior Contributor V
Dear Leo_A,

The API for the TBDML is described in the Zip file in the first posting of this thread:
http://forums.freescale.com/freescale/board/message?board.id=TBDML&thread.id=2

However, it doesn't sound like you are using a TBDML cable (it's USB not serial)?  If not then I would suggest you post in the Codewarrior forums rather than here as you are more likely to receive a useful response.  Also identify the cable you are using as the interface DLL would vary.  AFAIK there isn't a higher-level more uniform API available.

bye



0 Kudos
Reply