an error comes out when I use USBDM programmer to program MC9S08DZ60.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

an error comes out when I use USBDM programmer to program MC9S08DZ60.

1,827 Views
wangbaode
Contributor IV

Dear pgo,

when I program MC9S08DZ60 through usbdm programmer,the error comes out.

pastedImage_0.png

I don't know why.can you give me advice to resolve the question?

bye

Tags (3)
0 Kudos
Reply
3 Replies

1,571 Views
pgo
Senior Contributor V

Hi Wang,

No idea.

I don't have a DZ60 for testing.  I have tried similar devices (DZ128 & DV60) and they both work well.

Can you provide information about :

  • USBDM version
  • Hardware version.

You can try running the debug version of the programmer

     HCS08_FlashProgrammer-debug.exe

which will create a log file:

     $APPDATA%/USBDM/FlashProgrammer_HCS08.log

which might have some clues.

bye

0 Kudos
Reply

1,571 Views
wangbaode
Contributor IV

Hi pgo,

the error does not always come out. just on the special board ,it comes out.

can you tell me which condition casue the error?

0 Kudos
Reply

1,571 Views
pgo
Senior Contributor V

Hi Wang,

The message just indicates that some function in the TCL script used to initialise or erase the target has failed.  The log mentioned above may have mode information,

bye

0 Kudos
Reply