What is the difference between osbdm and usbdm? Is OSBDM open source?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the difference between osbdm and usbdm? Is OSBDM open source?

5,487 次查看
andy_Musk
Contributor III

What is the difference between osbdm and usbdm? Is OSBDM open source? Where can I find the information.

0 项奖励
回复
10 回复数

5,444 次查看
andy_Musk
Contributor III

where can i get the hardware and software information about OSBDM?
hardware and software information about OSBDM is open source?

0 项奖励
回复

5,475 次查看
pgo
Senior Contributor V

USBDM is hardware and software designed my me.

https://sourceforge.net/projects/usbdm/

https://github.com/podonoghue/usbdm

https://usbdm.sourceforge.io/USBDM_V4.12/html/index.html

 

The early version of OSBDM was an opensource community effort I believe.  It was later updated more officially by Freescale.  The hardware description is opensource but I believe the firmware was written by P&E and I am unsure if it is available.

Note these are not interchangeable but in some limited roles the USBDM 'pretends' to be an TBDML/OSBDM for compatibility with Freescale software.  The software you have been trying to use (e.g. memory dump) only works with USBDM.

0 项奖励
回复

5,428 次查看
andy_Musk
Contributor III

the USBDM is an open source project? where to get the source code of USBDM?

0 项奖励
回复

5,413 次查看
pgo
Senior Contributor V

???

Refer to earlier post

 

0 项奖励
回复

5,398 次查看
andy_Musk
Contributor III

not find the source code.just have many exe files and *.sx firmware!

0 项奖励
回复

5,392 次查看
pgo
Senior Contributor V

There are three links given.  Did you look at all three? A really really hard look?

 

0 项奖励
回复

5,346 次查看
pgo
Senior Contributor V

For Example: (from 3rd link you provided):

https://github.com/podonoghue/usbdm-firmware

The above is a GIT repository containing source for the flash routines used on the target processors.

https://github.com/podonoghue/usbdm-eclipse-makefiles-build

The above is a GIT repository containing source for application programs.

What does "I cannot open it" mean?

Are you having trouble with them being GIT repositories?

You can download a ZIP from code button:

pgo_0-1686927721813.png

 

0 项奖励
回复

5,324 次查看
andy_Musk
Contributor III

usbdm-eclipse-makefiles-build-master.zip: Corrupt compressed file

0 项奖励
回复

5,305 次查看
pgo
Senior Contributor V

Works for me - just tested.

I imagine if GITHUB had a problem with ZIP downloads you would not be the only one experiencing problems - It is used by 1000's of users.

Check you system.

bye

0 项奖励
回复