USBDM Ubuntu - Device no responding or busy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USBDM Ubuntu - Device no responding or busy

跳至解决方案
1,284 次查看
MartinKupec
Contributor II

Hi, I am using USBDM on Ubuntu 14.4. When I plug it in and open HCS08_FlashProgrammer. It detect my programer and prints right firmware version. But any other action (e.g. "Detect" button) results in "Device no responding or busy" and random firmware version. Any idea what can be wrong? The same USBDM works on windows. I am using last software from sourceforge (tried both 32/64-bit versions)

0 项奖励
回复
1 解答
1,051 次查看
pgo
Senior Contributor V

Hi Martin,

Would you mind re-testing on the current version V4.11.1.40?

Thank you

在原帖中查看解决方案

6 回复数
1,051 次查看
MartinKupec
Contributor II

I have just tried it with different versions of libusb on different computer and it is the same (1.0.8, 1.0.11, 1.0.19). Also I have tried different USBDM hardware.

I am using usbdm_4.10.6.240-1-amd64.deb. Non of it makes any difference.

Any chance of releasing 4.11 for linux, to give it a try?

0 项奖励
回复
1,051 次查看
pgo
Senior Contributor V

Hi Martin,

I'm currently working on the Linux version so a good time for testing

Can you tell me the BDM hardware types you have tested?

bye

0 项奖励
回复
1,051 次查看
MartinKupec
Contributor II

I am not exactly sure, but I believe I have USBDM_JS16CWJ and USBDM_SWD_JS16CWJ

The second one is for sure. I am trying to flash HCS08 and Kinetis devices. I have flashed to both dongles current firmware (that one that comes with the software).

I did it on windows, as it wasn't possible to do in on linux because of the problem I am having

0 项奖励
回复
1,052 次查看
pgo
Senior Contributor V

Hi Martin,

Would you mind re-testing on the current version V4.11.1.40?

Thank you

1,051 次查看
MartinKupec
Contributor II

Sorry it took so long. I needed to finish different project.

I can confirm, that 4.11.1.60 works on linux flawlessly.

Thank you

1,051 次查看
pgo
Senior Contributor V

Hi Martin,

Thank you for testing

bye.

0 项奖励
回复