USBDM Ubuntu - Device no responding or busy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBDM Ubuntu - Device no responding or busy

ソリューションへジャンプ
1,205件の閲覧回数
MartinKupec
Contributor II

Hi, I am using USBDM on Ubuntu 14.4. When I plug it in and open HCS08_FlashProgrammer. It detect my programer and prints right firmware version. But any other action (e.g. "Detect" button) results in "Device no responding or busy" and random firmware version. Any idea what can be wrong? The same USBDM works on windows. I am using last software from sourceforge (tried both 32/64-bit versions)

0 件の賞賛
返信
1 解決策
972件の閲覧回数
pgo
Senior Contributor V

Hi Martin,

Would you mind re-testing on the current version V4.11.1.40?

Thank you

元の投稿で解決策を見る

6 返答(返信)
972件の閲覧回数
MartinKupec
Contributor II

I have just tried it with different versions of libusb on different computer and it is the same (1.0.8, 1.0.11, 1.0.19). Also I have tried different USBDM hardware.

I am using usbdm_4.10.6.240-1-amd64.deb. Non of it makes any difference.

Any chance of releasing 4.11 for linux, to give it a try?

0 件の賞賛
返信
972件の閲覧回数
pgo
Senior Contributor V

Hi Martin,

I'm currently working on the Linux version so a good time for testing

Can you tell me the BDM hardware types you have tested?

bye

0 件の賞賛
返信
972件の閲覧回数
MartinKupec
Contributor II

I am not exactly sure, but I believe I have USBDM_JS16CWJ and USBDM_SWD_JS16CWJ

The second one is for sure. I am trying to flash HCS08 and Kinetis devices. I have flashed to both dongles current firmware (that one that comes with the software).

I did it on windows, as it wasn't possible to do in on linux because of the problem I am having

0 件の賞賛
返信
973件の閲覧回数
pgo
Senior Contributor V

Hi Martin,

Would you mind re-testing on the current version V4.11.1.40?

Thank you

972件の閲覧回数
MartinKupec
Contributor II

Sorry it took so long. I needed to finish different project.

I can confirm, that 4.11.1.60 works on linux flawlessly.

Thank you

972件の閲覧回数
pgo
Senior Contributor V

Hi Martin,

Thank you for testing

bye.

0 件の賞賛
返信