USBDM 4.12.1.150 can´t program MC9S08JM60CLD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBDM 4.12.1.150 can´t program MC9S08JM60CLD

1,532 Views
lucianonicolau
Contributor III

Hi pgo,

please check the 4.12.1.150 because it can´t program the MC9S08JM60CLD. The programmer can detect chip but can´t program or erase it, returns TCL error when try "mass erase now" or "program flash" I loaded the flash image USBDM_JMxxCLD_V4.sx from FlashImages folder. The option "verify flash" works fine. I am using windows7 64bits. I try some commands on TCL interpreter and it works. 

Labels (1)
0 Kudos
Reply
1 Reply

1,243 Views
pgo
Senior Contributor V

Hi Luciano,

I have located the error and uploaded a revision.

bye

0 Kudos
Reply