TBDML Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TBDML Error

3,713 Views
admin
Specialist II
I implemented a TBDML BDM on a DT256 target board aimed at the Educational arena.  However, when I attempt to use CW for HCS12, V4.6 I get the following error:
 
"Unknown Device: The connected device PARTID/SDID (0x0033 is not registered in the debugger core file.  Do you want to select the device from a list?) 
 
I click okay, pick from the list and it works..but it will prompt me again next time.  I can erase and program the target using a P&E Multilink and the P&E tools.  The program runs as expected.  Howver, when I attempt to program the device using CW and the Multilink cable programming fails. 
 
Since the part can be programmed using the P&E tools and the P&E cable I have to assume the board design is OK.  I believe this is a CW problem either with the setup or with program functionality but I don't know where to look.
 
Any thoughts?
 
Thanks
 
 
0 Kudos
Reply
1 Reply

1,259 Views
Nabla69
Contributor V
Hello Spencer,

The TBDML has no trouble with S12 and does not use a different list of PARTID from the other tool.
I see two choices for you:

- Check your communications parameters and see if 0x0033 is the right PARTID for the DT/DG256.
- Ask support from FSL direct because you are a partner...

Cheers,
Alban.
0 Kudos
Reply