Source for CFV1_FlashProgrammer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Source for CFV1_FlashProgrammer

2,763 Views
ianleonard
Contributor I

Where can I find the source code for CFV1_FlashProgrammer for Linux?

Thanks

Labels (1)
0 Kudos
Reply
4 Replies

2,310 Views
pgo
Senior Contributor V

Dear Ian,

The Linux version is rather out of date but I am currently updating it.

The latest Linux source code available is:

http://sourceforge.net/projects/usbdm/files/Version%204.5/2.%20Source_4_5/

Eventually I will redo the GIT repository with a Makefile based version that should build under both windows and Linux (at least one of em).

bye

Update:

The current Linux sources and binary files have been uploaded to sourceforge.

USBDM - Browse /Version 4.10.3 at SourceForge.net

bye

0 Kudos
Reply

2,310 Views
ianleonard
Contributor I

Hi Peter,

Is there a 4.10.3 version of the bdm firmware available? I can only find 4.10.2.

Thanks

Ian

0 Kudos
Reply

2,310 Views
pgo
Senior Contributor V

Hi Ian,

The BDM firmware for JMxx & JS16 is available at the same page:

http://sourceforge.net/projects/usbdm/files/Version%204.10.3/Source/USBDM_JMxx_V4_10_3%2812_10_23%29...

This should agree with the binaries posted.

This is a Codewarrior project. It should build unchanged under linux & windows.

bye

0 Kudos
Reply

2,310 Views
ianleonard
Contributor I

Hi Peter,

Just to say thank you for the source code. I have just built it (after a few xw related problems).

Ian

0 Kudos
Reply