Problem with PEMicro Virtual Serial Toolkit (TWR-MCF5441x board)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with PEMicro Virtual Serial Toolkit (TWR-MCF5441x board)

1,420 次查看
magicmarmot
Contributor I

I have a Tower setup with the SER2 module and the MCF5441x (coldFire) board. The board has updated firmware (31.21), the PEMicro USB drivers  are up-to-date as well.

PEMicro_driver_ver.png

PEMicro_driver_ver_COM3.png

PEMicro_ident.png

With the board connected, I can see the drivers in Device Manager (Win7 64-bit), and all looks good.

I've been having difficulty with Code Warrior for MCUs 10.5 in downloading anything to the target board, and it seems to be based around the communication with the on-board OSBDM/debug USB port.

If I use the P&E virtual serial toolkit, it shows that I can successfully open the serial port (COM3), but the demo does not have any function.

PEMicro_VirtualSerialToolkit_open.png

If I try the serial re-director, I get the error message "Failed to Open Multilink USB. Plug DEMO board into PC via USB cable.

Anybody have any ideas?

标签 (1)
0 项奖励
回复
0 回复数