OSBDM Bugs - Who to send fixes to?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OSBDM Bugs - Who to send fixes to?

3,395件の閲覧回数
pgo
Senior Contributor V
Dear All,

I've found what I believe are some bugs in the OSBDM code.  To whom should fixes be directed?

Summary:

The following Low level BDM routines are incorrect (They all expect ACKN which does not occur for these commands,  This ends up disabling the ACKN operation):

BDM08_CMD_READSTATUS
BDM08_CMD_WRITECONTROL
BDM08_CMD_READ_BKPT
BDM08_CMD_WRITE_BKPT

bye
ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

803件の閲覧回数
osbdm_support
Contributor II
Hi pgo,

You can send your fixes to me for review.

Thanks!

Dan

0 件の賞賛
返信

803件の閲覧回数
pgo
Senior Contributor V

Dear Dan,

Attached is a text file that lists what I believe are some minor bugs in the OSBDM code.

The example code is from the USBDM code posted elsewhere so does not correspond exactly with the changes needed in OSBDM but should be sufficient to indicate what to look at.

Please let me know if anything is unclear or if I am mistaken.

Bye

 

Fixes1.txt

Message Edited by t.dowe on 2009-10-26 05:07 PM
0 件の賞賛
返信