Linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux

6,019 次查看
ben106
Contributor I
Hi,
is it possible to program the microcontroller with Linux ? (I mean Linux on the computer, not on the microcontroller)

And if so, is "live debugging" possible ?

Thanks

Ben
标记 (2)
0 项奖励
回复
4 回复数

2,556 次查看
AceMax
Contributor I

Raise it again!

 

Same question.

0 项奖励
回复

2,556 次查看
greg_b
Contributor I

For now use a virtual machine like VirtualBox.

 

The osbdm-jm60 is an open source driver, sonner or later someone will rewrite it for the GNU/Linux.

0 项奖励
回复

2,556 次查看
admin
Specialist II

Hi

 

I am very interested in doing the same thing. Here is a link which may or may not be usefull:

 

http://www.sparetimelabs.com/funwith08/funwith08.html

0 项奖励
回复

2,556 次查看
BradR
Contributor I
I see that this question has never been answered, so I'd like to raise it again. Is there any support under Linux for the OSBDM08?

Failing that, is there source code available for the PC end of the OSBDM08? I've looked in this forum but so far haven't found any links to the OSBDM08 software. It's possible that a port to Linux would be straightforward.

Message Edited by Brad R on 2008-12-12 10:41 AM
0 项奖励
回复