JS16 OSBDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JS16 OSBDM

1,870件の閲覧回数
Michael_Theisse
Contributor I

Hallo,

 

refering to USBDM_SOIC_JS16(Minimal):

 

Is it right that BKGD_DRV is connected to input- and output pins on MC9S08JS16CWJ. BKGD_DRV drives only an input pin on U1B (74LV125AD)?

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,048件の閲覧回数
pgo
Senior Contributor V

Dear Michael,

 

The connections are correct.

 

The two pins are used as outputs to control the buffer at different times with the other pin 3-state.  Neither is actually used as an input.

 

This allows for faster manipulation of multiple port pins on a shared port but also allows independent control using a separate pin.

 

bye

 

0 件の賞賛
返信