Creating KeyFob Programmer - OSBDM JM60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating KeyFob Programmer - OSBDM JM60

1,721件の閲覧回数
bob1_2
Contributor I

Hi all,

 

I am using the 9RS08KA1 microcontroller and wish to design a keyfob programmer. I understand that there is an open soucre BDM available that can be used to design a programmer for the rs08. However i want a storage mechanism, so would i be able to store my own data/program in the internal flash of the JM60??

 

has anyone else done this sort of thing? and is there any firmware/source code to go with the OSBDM.

 

If anyone could help would greatly appreciate it.

Thanks.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)