NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
Detailed training session on developing with the LPCXpresso Ecosystem, showing the main features of the tools, from project import/creation, multi-core debug and power optimization. The LPCXpresso boards and IDE toolchain will be used with the latest version of LPCOpen peripheral driver examples. We will cover some cool new features including trace and power analysis.
View full article
This session will provide an overview of the QorIQ security accelerator block, its device driver, and its use in IPsec and SSL acceleration. Watch Video Presentation
View full article
Learn how Qt for Device Creation may be used to create advanced user interfaces in a few simple steps. Qt is a cross-platform C++ framework that offers tools to create modern and fluid user experiences. The Qt framework may utilize the OpenGL ES capable i.MX6 or perform simplified rendering for the new i.MX7. We will take a look at Qt and use Qt for Device Creation to develop a GUI application optimized for projects requiring low power and real-time tasks which are suitable for wide-range of industrial applications, while keeping advanced security features to be used in IoT applications—all with confidence and convenience. Attendees will discover how easily it is to enable a low power device with performant GUI effects. This evolution requires virtually no changes to the software or hardware -- made possible by the Qt Framework and standardized pin-compatible computer modules from Toradex.
View full article
IoT applications often share some basic requirements; the applications themselves need to be small, fast and low-energy, while the time to market should be as short as possible. To help you meet these demands, a wide range of possibilities and techniques for performing smart debugging of code is actually already at your fingertips. At this session you will learn how to use debug features like various types of complex breakpoints, macros, stack checking, event logging, live data, profiling and runtime code analysis in a smart way for comprehensive debugging of your code.
View full article
One particular wave of innovation in the world of ARM is an increase in heterogeneous CPU designs, where different classes of ARM processor are implemented on the same device. NXP are at the forefront of this wave. For example the i.MX 7 family of devices implement both a Cortex-A7 application processor and a Cortex-M4 embedded processor. In this session we will discuss the challenges that such a design brings to a developer, as well as how with DS-5, ARM gives you a powerful tool to address them.
View full article
Electronics are part of everything we do nowadays, whether we are talking about mobile gadgets or a space rocket. Regardless of the complexity of the products designed, at some point, they have to be brought to actuality, so they have to be manufactured. This session addresses the impact of some of the most important printed circuit board attributes that affect quality, cost, and lead time.
View full article
This session will feature the LPC54114 MCU, the latest release of the LPC54000 low-power series, to demonstrate how to take advantage of dual-core architecture in always-on applications. Optimize product design for extended battery life and bring them to market quickly with this hands-on session. Topics will range from system architecture, software design and debugging, to power optimization, sound detection, and voice triggering.
View full article
We will walk you through the key features of the LPC800 and LPC1100 product series and how these low-power, low-cost MCUs bring numerous advantages over your 8-bit architecture. In this session, we will discuss bridge from 8-bit to 32-bit applications using the LPC800 and LPC1100. Customers can expect 8-bit simplicity, real-time performance, and better code density with easy-to-use tools while maintaining lower power at a much lower cost. NXP delivers all the key ingredients that embedded engineers need for successful USB application development. Watch Video Presentation
View full article