eMMc for LS1088A design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMc for LS1088A design

1,818件の閲覧回数
Giang
Contributor I

I am designing a schematic using the LS1088A solution.

Currently, the eMMC lines recommended by NXP all have EoL, we are looking for a solution to replace them.

What types of eMMC are compatible with the LS1088A chipset? Can NXP provide suitable eMMC electrical specifications or alternative eMMC part?

Thanks

1 返信

1,778件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The LS1088a eSDHC is compatible with the eMMC system specification version 4.5. It supports SDR50 and eMMC high speed HS200 mode.

 

The eMMC device should be compatible with the eMMC system specification version 5.1. It also supports SDR50 and eMMC high speed HS200 mode.