TJA 1145 Lock register, locking by default

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA 1145 Lock register, locking by default

3,853 Views
rajarajan_m
Contributor I

We are using TJA 1145 TK CANFD Cantranciever. 

We expect the CANTrcv configuration values (PN Id, PN Mask etc.) to be written into the various CANTrcv registers during the call of CANTrcv_Init(). However upon reading the corresponding registers after the CANTrcv_Init() call, these registers were not filled with the configured values. Upon checking, we saw that the the bits in the Lock Control register (Address 0x0A) was set such that no data can be written. Further there is no option in our Tranciever driver configuration to unlock the same.

I understand that the default state of the lock register is Unlock after Power on, however it does not seem to be the case for us.

Please support on how to handle the same case.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

3,710 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Rajarajan, 

please click at the link where you can find and download a software examples for TJA1145 tranciever. 

Best regards Jozef

0 Kudos
Reply

2,896 Views
yesuyi
Contributor I

Can you send me a link again? The previous one is not working.

0 Kudos
Reply