T4240

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T4240

34 次查看
wutongxue
Contributor I

Does Aurora support data communication as a high-speed port?

0 项奖励
回复
6 回复数

21 次查看
yipingwang
NXP TechSupport
NXP TechSupport

If by Aurora you mean the Xilinx/AMD Aurora 8B/10B or Aurora 64B/66B serial link protocol, then no, T4240 does not natively support Aurora as a high-speed communication interface.

For a new T4240 ↔ FPGA design requiring high throughput, I would normally select PCIe Gen3 rather than Aurora.

0 项奖励
回复

9 次查看
yipingwang
NXP TechSupport
NXP TechSupport

No—not for general-purpose high-speed data communication. The T4240 SerDes4 Aurora interface is intended for debug/trace, not as a replacement for the FPGA’s application-data Aurora link.

Keep the FPGA as the Aurora-to-optical endpoint and connect the T4240 to it through PCIe, SRIO, or Ethernet.

0 项奖励
回复

6 次查看
wutongxue
Contributor I
If I want to communicate using AURORA, is it possible? Does the T4240 support communication via AURORA?
0 项奖励
回复

5 次查看
yipingwang
NXP TechSupport
NXP TechSupport

NXP's application note AN4933: Aurora Trace for CodeWarrior Power Architecture describes Aurora as a SerDes communication channel used to extract Nexus trace data from processors that support the Aurora trace interface. It works with the CodeWarrior Gigabit TAP + Trace/Aurora daughter card.

So if by “communication” you mean:

Can my application on the T4240 use its Aurora interface as a general-purpose high-speed data link to another processor or FPGA?

I would say No, not using the T4240's Aurora trace port as a normal application communication peripheral.

0 项奖励
回复

3 次查看
wutongxue
Contributor I
ok,I see,thankyou
0 项奖励
回复

12 次查看
wutongxue
Contributor I
The T4240 manual shows that serdes4 can be configured for AURORA. Our current setup has the FPGA connecting to an optical module via AURORA. Can the T4240 connect to the optical module via AURORA for high-speed communication? If yes, how should it be implemented?
0 项奖励
回复