Hi @Senlent
Greeting for the day ..!!
i am currently working on S32k342 microntroller and as per the website the S32 design studio for s32 platform v3.5 is downloaded but i am unable to find the SDK for the S32K342 series. kindly guide to proceed in downloading it..
解決済! 解決策の投稿を見る。
I am sorry that the installation problem has troubled you, I have summarized my installation process, you can refer to it.
1.download highlight parts.
2.open S32 DS V3.5 ->Help->Install New Software,
After the installation is complete, restart S32 DS V3.5, and you should be able to use it.
If you still have problems related to install this software, please contact me in time, and I will help you solve them in time.
first, you need to sign on NXP webpage.
1.then:
2.
3. S32K3 Real Time Drivers Version 2.0.0
Hi @Senlent,
I would like to thank you for the reply @Senlent.
As per the reply i have downloaded the S32K3 Real Time Drivers Version 2.0.1 .exe file and the installation is done while installing EB Tresso studio linker path is left blank since i have no EB Tresso studio to link. I find no difference in installing RTD is there any further steps to be done ,kindly help to proceed further.
Thanks and regards,
Ganesh pawar
Update:
I found some describtion related to your question:
Release Notes for S32K3 RTD Version 2.0.1.pdf
1.3 Installation EB Tresos
Follow the installer steps. By default the installer will create a link between the installation target directory and a selected EB Tresos installation. If you choose not to create a link, you can later create one manually or you can copy all "_TS_T40D34M20I1R0" directories and .JAR files to the "\plugins" directory.
The S32K3 Real-Time Drivers Version 2.0.1 is AUTOSAR 4.4.0 compliant. The
AUTOSAR Configuration ARXML specification takes precedence over AUTOSAR SWS
PDF Specifications if there are discrepancies.
The S32K3 Real-Time Drivers Version 2.0.1 can be used also in non-AUTOSAR
environment, as a collection of peripheral drivers designed to simplify and accelerate
application development on NXP microcontrollers.
Please check whether you can use S32 DS V3.5 to compile the provided demo project, if everything is normal, please ignore this step.
If S32 DS V3.5 cannot compile the provided demo normally, please tell me, because I did not choose your installation method, I will tell you the steps of my installation.
Regarding EB software, this is also a software tool we provide to customers, which can be used to compile MCAL
BR!
Hi @Senlent ,
Greetings for the day..!!!
I have created the application project with S32K342 controller in the S32 DS for S32 platform v3.5 the selection of SDK is unavailable (empty, as per the file attached ), After the installation of RTD driver is there any steps to map to the existing controller. if i am able to select the SDK for the same, my problem is solved and proceed to utilize it Kindly help to proceed further.
PS: Is it necessary to install the EB tressos studio.
Note: S32K116-SDK.png is attached just for the reference for selection of SDK.
Thanks and Regards,
Ganesh Pawar
I am sorry that the installation problem has troubled you, I have summarized my installation process, you can refer to it.
1.download highlight parts.
2.open S32 DS V3.5 ->Help->Install New Software,
After the installation is complete, restart S32 DS V3.5, and you should be able to use it.
If you still have problems related to install this software, please contact me in time, and I will help you solve them in time.
Hi @Senlent ,
Greetings for the day...!!!
Thank you very much for your time and guidance really appreciate it, I have the SDK file as per your installation guide really helped me to get it .
Before i conclude i have a querry regarding the EB tressos studio is it really required to install for the usage of the S32K3xx family controllers.
Thanks and regards
Ganesh Pawar
This is not a requirement,
RTD provides customers with autosar and non-autosar two development methods. For customers who have autosar needs, they can use either EB or S32 DS.