PTN3460 support EPI ( Embedded Panel Interface ) EDID?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3460 support EPI ( Embedded Panel Interface ) EDID?

6,055 Views
dylan_lin
Contributor III

EPI panel paremeters register since  0x71h~0x7Dh

PTN3460 panel parameters register since 0x80h~0xEC

 They were not conflict at register address , so PTN3460 can support EPI ?

 

0 Kudos
Reply
6 Replies

6,007 Views
dylan_lin
Contributor III

Hi Jozef ,

Thanks your reply ,

I have checked some EPI control display parameters from 0x71H~0x7DH,  the PTN3460 control display parameter 0x80H~0xECH,

both all in the  universal 128Kbyte data and does not  conflict, if i want use to PTN3460 to control EPI panel , can i use EPI display parameter or

use PTN3460 control parameter ?

0 Kudos
Reply

6,002 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Dylan,

please share a datasheet of the display you are using with the PTN3460.

With Best Regards,

Jozef

0 Kudos
Reply

5,962 Views
dylan_lin
Contributor III

Hi Jozef ,

i dont have datasheet of Display , i have EPI spec , because i am studying EPI interface , so i want to know if PTN3460 can support it ? And where the real application should pay attention.

5,922 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Dylan,

ok. I have sent your reply with the EPI specification document to the application engineer. So far I haven't received an answer from him. As soon as he answers me, I will definitely reply to you. Thank you for your patience.

With Best Regards,

Jozef

5,885 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Dylan,

Still no answer from the application engineer. I have just sent him a reminder. Hopefully he will answer me soon.

With Best Regards,

Jozef

0 Kudos
Reply

6,008 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Dylan,

please see below an answer from an application engineer I have contacted.

DESCRIPTION

PTN3460/3460I do support VESA EDID 1.3, as long as EPI standard is compliant with VESA EDID V1.3, then PTN3460/3460I can support it.

Can you explain more detail about “EPI panel parameters register since 0x71h~0x7DhPTN3460 panel parameters register since 0x80h~0xEC They were not conflict at register address, so PTN3460 can support EPI? “ I don’t understand what is the question?

With Best Regards,

Jozef

0 Kudos
Reply