NTS0104 internal pull-up resistor, output voltage accuracy

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTS0104 internal pull-up resistor, output voltage accuracy

2,061 Views
akihiro_yamada
Contributor I

1. Please tell me the tolerance of 10kΩ internal pull-up resistor of B port.

2. If the current source of B port is only 10kΩ internal pull-up resistor, which does output voltage tolerance depend on VCC or 0.67VCCO?

Tags (2)
0 Kudos
Reply
2 Replies

2,004 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

1:Tolerance is about +-20%

2: You can check datasheet page8 table9 for VOH/VOL specification.

0 Kudos
Reply

2,004 Views
akihiro_yamada
Contributor I

Dear G.w. Sun,

Thank you for your reply.

Problem solved.

Best regards,

0 Kudos
Reply