MRFX035H S-Parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRFX035H S-Parameters

1,202 Views
Stephan_Orzada
Contributor I

I have a question regarding the S-parameters provided for the MRFX035:

I had used the S-paramters to match the MRFX035H to 300 MHz, but when I use the resulting circuit in real life, the matching is completely off. Are the S-Parameters provided on the web-page actually correct?

When I simulate the 230MHz reference board from the Datasheet using the S-parameters, the results show that it is matched for ~300 MHz. So something seems to be wrong there.

I'm using this file:

! 12/17/2018
! Rev 0
! MRFX035H S-Parameters
! Vdd=65V, IDQ=150mA

0 Kudos
Reply
0 Replies