MRF101AN NEAR FM BAND PERFORMANCE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MRF101AN NEAR FM BAND PERFORMANCE

1,847 次查看
silicontechnolo
Contributor I

MRF101AN: 100 W transistor. 

Regarding reference circuit 87 to 108 Mhz.. can i use it at 76 to 87 Mhz? what is the frequency response in that band? output power? If not, can NXP support in modifying component values ( I want to use ready kit)in reference design?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,777 次查看
LPP
NXP Employee
NXP Employee

Reference circuit 87 to 108 Mhz would require some tuning to be used in your target frequency range.
You have created support ticket #00266185 on this topic. I will continue discussion there.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复