MHT2012N biasing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MHT2012N biasing

1,611 Views
tpraveen_uts
Contributor I

Hi,

pastedImage_1.png

Can anyone explain it clearly ?

0 Kudos
Reply
1 Reply

1,570 Views
LPP
NXP Employee
NXP Employee


In a well designed, stable circuit, the LDMOS is sequencing indifferent. One can bring up the RF, Gate and Drain tabs in any sequence and the part will amplify as originally intended. A designer must check that the design remains stable in power transient conditions.

In the case of NXP reference circuit, the quiescent currents is determined by separate gate voltage supply. The recommended quick start sequence prevents possibility of unwanted high drain current when the gate supply voltage is too high and if it starts before the drain supply.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply