ECC Change Regression testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ECC Change Regression testing

2,531件の閲覧回数
scnaidu
Contributor II

We have run into a regression on the ECU(SPC58NN84C3) that we believe is related to the changes for the ECE reset enablement.  The issue we are seeing is the ECU(SPC58NN84C3) will continuously reset when jumping to the bootloader.  The reset appears to be coming from the SBC (FS85),

The diagnostic from the SBC reads: upper 32 bits: 0xF920 and the lower 32 bits: 0x410000

 

We have developed E2E ECC 1bit and 2bit error into sram, with FCCU channel configuration (EOUT signal Enable) and SBC configuration chnage FS8X_FS_I_FCCU12_FS_IMPACT_FS0B_RSTB

E2EECC was called in 10ms tasks.

@petervlna  please support needed asap

ラベル(1)
0 件の賞賛
返信
0 返答(返信)