Build basic production material tracking application with NFC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build basic production material tracking application with NFC

1,473 Views
mortpiedra
Contributor I

We are a small company and have no experience with NFC yet, but wish to build a basic production material tracking application with the help of NFC technology (as opposed to using barcodes and scanners).

My very basic research makes me believe that we need the following NFC tags:

- must support low temperatures -20C

- ISO 15693 (since the reading distance will be about 30cm)

- ideally integrated in thick PVC-card of credit card size

- writeable in order to accomodate an 8 character product code

- write protection basic (only in order to prevent accidental change of above product code)

- number of required tags: 500

- the tags will be placed in stainless steel containers (25X30X15cm) and will be read from above

Any assistance with how/where we could get a hold of tags in this format would be greatly appreciated.

One option for us would be to hire a technology company to provide the entire solution from start to end inlcuding suppling of the tags, but we afraid that we could not carry the cost.

Thank you.

Mort

P.S. I choose 'NXP Designs', but have no idea what woud be a proper location, so please do not hesitate to letting me know if I should move it. 

0 Kudos
Reply
1 Reply

1,443 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 You may refer to the products as the link.ICODE® | NXP 

Hope it help you. Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply