BFU590

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BFU590

1,742 Views
qiang-liu
Contributor I

can BFU590  be used in short wave band?

0 Kudos
Reply
1 Reply

1,696 Views
LPP
NXP Employee
NXP Employee

BFU590 can be used from DC to 2GHz.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply