2 Questions about FlexRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2 Questions about FlexRAM

ソリューションへジャンプ
7,460件の閲覧回数
kmh48301
Contributor IV

Hi. I'm using S32k144.

But the forum dosen't work for me. so I'm posting here.

 

1. FlexRAM is slower than SRAM

 

Please see the attachment. (it's from AN11983 p11)

 

When I see flash memory map, I think FlexRAM is also contiguous addresses.

but this is saying non-contiguous...

and is that why the FlexRAM is slower than SRAM?

FlexRAM is not static RAM (SRAM)?

 

2. "a background pattern of all ones" ???

I saw "a background pattern of all ones" several times in NXP documents..

But I have no idea what it means since I'm not native English speaker,,

 

 

Please explain to me

 

Thanks

Best regards,

Phillip

ラベル(1)
0 件の賞賛
返信
1 解決策
7,430件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

1. This is given by architecture, not by the RAM itself. As you can see, the memories are sitting on different places which inserts some difference:

lukaszadrapa_0-1599466625438.pnglukaszadrapa_0-1599466625438.png

2. "background pattern of all ones"  means, that memory controller will initialize all bytes in FlexRAM allocated for EEE to "0xFF" (all ones) and then it will copy down valid data/records from backup flash. So, non-written words have default value 0xFFFFFFFF.

Regards,

Lukas

 

 

元の投稿で解決策を見る

3 返答(返信)
7,417件の閲覧回数
kmh48301
Contributor IV

Thank you so much. i thought wrong way. hahaha

0 件の賞賛
返信
7,457件の閲覧回数
kmh48301
Contributor IV

1.

kmh48301_1-1599099331237.pngkmh48301_1-1599099331237.png

 

2.

kmh48301_0-1599099302719.pngkmh48301_0-1599099302719.png

 

0 件の賞賛
返信
7,431件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

1. This is given by architecture, not by the RAM itself. As you can see, the memories are sitting on different places which inserts some difference:

lukaszadrapa_0-1599466625438.pnglukaszadrapa_0-1599466625438.png

2. "background pattern of all ones"  means, that memory controller will initialize all bytes in FlexRAM allocated for EEE to "0xFF" (all ones) and then it will copy down valid data/records from backup flash. So, non-written words have default value 0xFFFFFFFF.

Regards,

Lukas