Motor Control Development Toolbox with MATLAB™/Simulink™ Support - Demo

cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Control Development Toolbox with MATLAB™/Simulink™ Support - Demo

No ratings

Motor Control Development Toolbox with MATLAB™/Simulink™ Support - Demo

Demo Owner: b14714

The motor control development toolbox is a comprehensive set of tools that plug into the MATLAB™/Simulink™ model-based design environment for rapid application development on MCUs.  The SFIO Toolbox is a new addition that can control Simulink system models by SFIO algorithms running directly on NXP DSC and Kinetis MCU hardware. NXP FreeMASTER debug monitor and data visualization tool interfaces provide an interface to monitor signals in real time for data logging and signal calibration.

Features

  • The motor control development toolbox is a comprehensive set of tools that plug into the MATLAB™/Simulink™ model-based design
  • Auto code generation straight to the Micro. NXP developed a library and embedded target to interface with MATLAB and SimuLink
  • Customers can directly go from the model based environment to the MCU without having to write C code by hand


Featured NXP Products


Labels (1)
Comments

Where can I find the SFIO Toolbox as mentioned above?

I can only find the: Automotive Math and Motor Control Library Set

Version history
Last update:
‎07-11-2014 03:01 PM
Updated by:
NXP Employee