using 5180

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using 5180

2,477件の閲覧回数
larryansell
Contributor I

PN5180  NFC goes into a mode where all register reads return all FFs.  Two questions - how can I tell what in particular what I did that puts the chip into that mode, and is there any way to recover from it?  I see this happen on a second register read.

Thanks,

Larry

0 件の賞賛
返信
3 返答(返信)

2,300件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Could you please provide us with more information such as screen captures, Software Library Information, Host MCU...

Which register(s) are you specifically accessing to?

Thank you.

Regards,

Ivan.

0 件の賞賛
返信

2,300件の閲覧回数
larryansell
Contributor I

Hi Ivan,

Thanks for your reply. This turned out to be that I mistakenly had left another register read after the one where it seemed to be causing the lockup of all FFs. Now that is fixed.

However I do have another question please. I am trying to read and write a data card. Is it sufficient to have my code

1. Load a protocol

1. RF ON to energize the RF field

1. Load 3 into the SYSTEM CONFIG low bits 2:0 to start the transceive state machine

1. when I want to READ_DATA , no data has been received from the card,

Do I need to do anything else to start the reading? Similarly, do I need to do anything additional to get SEND_DATA to write data to the card?

Thanks for any help you can provide,

Larry

0 件の賞賛
返信

2,300件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

It would be helpful to refer to the examples available in the NFC Software Reader Library:

NFC Reader Library|NXP 

Regards,

Ivan.

0 件の賞賛
返信