pn532 p2p 0x13 error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn532 p2p 0x13 error

2,270件の閲覧回数
kimhyungjun
Contributor I

Hello
Please contact us as a 0x13 error occurred during the p2p test.

Logging data

-> SEND FIRMWARE

Senddata: 01 00 00 ff 02 fe d4 02 2a 00

Read data : 00 00 ff 06 fa d5 03 32 01 06 07 e8 00

Found chip PN532
Firmware ver 1.6
supports 7

-> SEND SAM 

Senddata: 01 00 00 ff 05 fb d4 14 01 14 01 02 00

Read data : 00 00 ff 02 fe d5 15 16 ff

-> SEND ATR 

Senddata: 01 00 00 ff 1e e2 d4 56 01 02 04 d5 15 16 ff ff 46 66 6d 01 01 11 02 02 07 80 03 02 00 03 04 01 32 07 01 03 d0 00

Read data : 00 00 ff 15 eb d5 57 00 01 01 fe 00 00 00 00 00 00 00 00 00 00 00 07 02 46 66 1f 00

-> SEND DEP

Senddata: 01 00 00 ff 05 fb d4 40 01 00 00 eb 00

Read data : 00 00 ff 03 fd d5 41 13 d7 00

Why am I getting a 0x13 error?

In the protocol, DID0x03 PFB is defined as 0x04.

 

 

 

 

 

 

0 件の賞賛
返信
3 返答(返信)

2,259件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the more information as the attachment. One may check your application with the SDK.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

2,254件の閲覧回数
kimhyungjun
Contributor I

I am using an NFC module V3 product.

Can I use this SDK?

Can you tell me about the internal implementation of phLibNfc_Hal_Transceive ?

github Is it okay to use C language lib-nfc?

0 件の賞賛
返信

2,243件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

There is the detail information in the SDK and you may refer to it.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信