mfrc630, clrc663 Change protocol problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mfrc630, clrc663 Change protocol problem

2,313件の閲覧回数
gksrb4
Contributor I

mfrc630, clrc663 Change protocol problem -> my old question .

I have developed mfrc630 and clrc663 pre-product. all these board read and write mifare card well.

But, another protocol didn't. even to change iso14443a data rates speed. 

My procedure is 

load protocol cmd -> cmd load(read eeprom and write registers) cmd

I check my registers, these are same as manual.

what should I start first?

ラベル(1)
0 件の賞賛
返信
1 返信

2,144件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Hangyu,

 

I'm not sure how are you deploying the command. Could you please look at UM10663 document?

 

You need to use the phhalHw_Rc663_ApplyProtocolSettings as well in the way it is explained in Chapter 2.1.13 LoadProtocol,

Note: Pay attention to the time configurations as those are not modified when using the commands.

 

Regards,

Mario

0 件の賞賛
返信