Writing data to NFC tag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing data to NFC tag

4,336 Views
yummy_ece03g
Contributor I

Hello, I need to program Data to 10K NFC TAGs. Also, I need to write different address for each TAG. Is there a writer or tool to recommend? Thx

Tags (1)
0 Kudos
Reply
4 Replies

3,625 Views
tinallen
Contributor I

I really like this, clean minimal, responsive just what i was looking for, cheers mate. McDVOICE

0 Kudos
Reply

4,227 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. There are some options. NXP has some developing tools for android that can help you, the NFC TagWriter by NXP would help you to write your tags.

 

Another option would be to use some of our readers. There is the NFC Reader Library that could help with your project.

 

Best Regards,

Ricardo

0 Kudos
Reply

4,227 Views
fred27murphy
Contributor II

The easiest would probably be something like NXP's TagWriter app for Android phones.

0 Kudos
Reply

4,227 Views
manuelbrooks50
Contributor I

Fred Murphy wrote:

The easiest would probably be something like NXP's TagWriter app for mcdvoice  phones.

But sir what can we do for ios app and other mobile os ?

Thank you

0 Kudos
Reply