Where to find command format and bytes for MIFARE PLUS SL0,1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where to find command format and bytes for MIFARE PLUS SL0,1

1,968件の閲覧回数
nc
Contributor II

After reading Mifare Plus product description document they mention commands and their names but not the actual format of the commands. For example APDU command type or something.

Where can I find this information ?

タグ(2)
0 件の賞賛
返信
1 返信

1,745件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to AN3764 MIFARE Plus EV1 Personalization Commands under NDA in DocStore.

I hope this helps.

Best regards,

Ivan.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信