Where is the code for AN12657

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the code for AN12657

ソリューションへジャンプ
2,308件の閲覧回数
Nik1
Contributor II

Where can I find the example code for AN12657? Been searching like a maniac without being able to find it. It's not in the NFC reader library as I thought it would be.

0 件の賞賛
返信
1 解決策
2,279件の閲覧回数
Nik1
Contributor II

I found it https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SW6693 . It's the "Anticollision register layer for CLRC663".

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
3 返答(返信)
2,289件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello, I appreciate your interest in our products.
We don't have any examples for this AppNote. The intention of this Application Note (Using the RC663 without library) is to show how to build and send the respective command set through a supported communication interface (SPI, I2C, I2CL, and serial UART).
Section 4 shows how to send the commands for either ISO 14443 or ISO 15693.
Using the Datasheet you can check the registers of the CLRC663 and, with the use of the respective ISO specification document the customer should be able to build the instructions for its application.
This application note is only for illustrative purposes and, does not have any examples.

Best Regards,
Fabian
0 件の賞賛
返信
2,281件の閲覧回数
Nik1
Contributor II

I see, I might have misunderstood. I think what I'm looking for may be the SW6693, RC663_Register_Example, I see it mentioned in several posts. For example "SW6693\RC663_Register_Example\Ex1_Simple_REQA". The reason I mentioned the AN12657 is because some months ago I'm pretty sure I downloaded some example code somewhere that names the functions the same way i.e. waitForCardResponse, writeRegister, readRegister.

0 件の賞賛
返信
2,280件の閲覧回数
Nik1
Contributor II

I found it https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SW6693 . It's the "Anticollision register layer for CLRC663".

タグ(1)
0 件の賞賛
返信