What is the NTAG213 antenna input maximum voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the NTAG213 antenna input maximum voltage

998 次查看
wilfrid
Contributor I

Hello all,

do you know what is the absolute maximum ratings for the antenna input for NTAG components.

My tag is submitted to a magnetic field of a Qi charger, I need to know the voltage limit that the tag may support, the only data in the datasheet is the maximum current, but at 100-200kHz this value is irrelevant.

Best regards,

Wilfrid

标签 (1)
0 项奖励
回复
1 回复

886 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Wilfrid,

The max current for RF input is 40mA, and max power dissipation is 120mW.


Wish it helps.

Have a great day,
Kan Li
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复