What does GSN stands for?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What does GSN stands for?

2,014 次查看
ahmedmomar88
Contributor I

What does GSN stands for? that is used in PN7150 and PN5180 as in:

TX_GSN_CW_CM      : GSN value for continuous wave in Card Mode
TX_GSN_MOD_CM   : GSN value for modulation in Card Mode
TX_GSN_MOD_RM   : GSN value for modulation in Reader Mode
TX_GSN_CW_RM      : GSN value for continuous wave in Reader Mode

Regards,

标记 (4)
0 项奖励
回复
1 回复

1,970 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi ahmed,

GSN here stands for the conductance of the output N-driver.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复