What does GSN stands for?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does GSN stands for?

1,983件の閲覧回数
ahmedmomar88
Contributor I

What does GSN stands for? that is used in PN7150 and PN5180 as in:

TX_GSN_CW_CM      : GSN value for continuous wave in Card Mode
TX_GSN_MOD_CM   : GSN value for modulation in Card Mode
TX_GSN_MOD_RM   : GSN value for modulation in Reader Mode
TX_GSN_CW_RM      : GSN value for continuous wave in Reader Mode

Regards,

タグ(4)
0 件の賞賛
返信
1 返信

1,939件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi ahmed,

GSN here stands for the conductance of the output N-driver.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信