Vdd for Pullup on FDpin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vdd for Pullup on FDpin

ソリューションへジャンプ
2,579件の閲覧回数
jesperselander
Contributor II

pastedImage_1.png

According to the specification on NTAG213F, max. Vdd for pullup on FDpin recommended is 3.6V. I am using a battery 3.3-4.2V as supply. Is that a problem?

Regards,

Jesper

0 件の賞賛
返信
1 解決策
2,455件の閲覧回数
jesperselander
Contributor II

Hi Jorge,

Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.

Best regards,

Jesper

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,455件の閲覧回数
jesperselander
Contributor II

Hi Jorge,

Thanks for your reply.

I assume  you mean keep VDD voltage below 4.6 V - please confirm.

Best regards,

Jesper Selander

0 件の賞賛
返信
2,455件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Jesper,

Sorry for the confusion. No, I meant keeping the voltage below 3.6 V, as specified in the datasheet:

FD_pin.png

Regards!

Jorge Gonzalez

0 件の賞賛
返信
2,456件の閲覧回数
jesperselander
Contributor II

Hi Jorge,

Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.

Best regards,

Jesper

0 件の賞賛
返信
2,455件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jesper Selander,

Actually the limiting value for voltage on the FD pin is 4.6 V. But as stated in the datasheet the exposure to limiting values for extended periods can affect device reliability, see below:

pastedImage_1.png

So I highly recommend you to keep VDD voltage below the 3.6 V.

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信