Using CLRC663 as P2P device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CLRC663 as P2P device

Jump to solution
187 Views
Tinvs
Contributor I

Hello,

We would like to use the CLRC663 plus as a Peer-to-peer (P2P) device. According to the datasheet the CLRC663 supports P2P mode according to the ISO/IEC 18092 in Passive Initiator mode.
This however brings up a multitude of questions:

  1. Is it possible to have two CLRC663 devices communicate with each other?
  2. If not, should the CLRC663 be combined with another device? Which is recommended?
  3. How to activate the ISO 18092 protocol? For other protocols I have found AN12657 at least describes how to activate some other protocols using the LoadProtocol functionality on the CLRC633, but the datasheet lacks any information on the ISO 18092 protocol. How these other two are activated is entirely unclear from the datasheet as well but can be inferred from this Application Note.
  4. Can two devices communicate in Passive Initiator mode?

I have looked at probably all posts already on the forum related to this but found nothing of use. I have also seen the NFC Reader Library but am unable to find anything useful regarding P2P.
Kind regards

0 Kudos
Reply
1 Solution
114 Views
Alondra
NXP TechSupport
NXP TechSupport

Hello, 

Please note that the Mikroe USB Dongle is not an NXP product. Therefore, application implementation and compatibility will depend entirely on the capabilities and support provided by the dongle manufacturer.

Additionally, the PN7150 is not recommended for new designs. NXP has discontinued Android maintenance for the PN7150 and does not plan to provide support for newer Android versions.

P2P communication based on ISO/IEC 18092 is being discontinued and is no longer supported by NXP.

A similar situation applies when considering two PN5190 devices. Since P2P is no longer supported, the recommended approach would be to configure one PN5190 as the NFC reader and the second device in card emulation mode, rather than implementing a P2P configuration.

For new designs, we recommend using currently supported NFC operating modes and solutions.

 

Best regards

View solution in original post

4 Replies
158 Views
Alondra
NXP TechSupport
NXP TechSupport

Hello,

Thank you for your interest in NXP Semiconductors products and for the opportunity to support you

CLRC663 is not fully NFC Forum compliant and it is intended for Reader/Writer mode. A CLRC663 can therefore be used with a different NFC device that supports the required target mode (i.e. HCE). For a standard ISO/IEC 18092 P2P connection, you could consider evaluating the PN5190.

However, this hardware consideration must also be evaluated together with the available support. Please notice that the NXP NFC Reader Library states that maintenance of its P2P functionality is being discontinued. Although earlier library releases include legacy P2P support, P2P functionality is not supported in our current software baseline.

 

Best regards, 

Alondra

0 Kudos
Reply
136 Views
Tinvs
Contributor I

Hello,

Thanks for your response.

We will look into the PN5190 as well.

We have a Mikroe USB Dongle which uses the PN7150, could this be used to test this functionality too?
My main concern is with setting the ISO 18092 standard on the CLRC663. For other protocols I have found the settings to enable this, but not for ISO 18092.

Would it be possible or perhaps easier to use two PN5190 ICs to let them communicate together? 

As a sidenote, it seems NFC P2P is sort of 'old school', Android stopped supporting it about 7 versions ago, and NXP it seems also treats it as legacy. Is this even worth trying? 

Kind regards

0 Kudos
Reply
114 Views
Alondra
NXP TechSupport
NXP TechSupport

Hello, 

Please note that the Mikroe USB Dongle is not an NXP product. Therefore, application implementation and compatibility will depend entirely on the capabilities and support provided by the dongle manufacturer.

Additionally, the PN7150 is not recommended for new designs. NXP has discontinued Android maintenance for the PN7150 and does not plan to provide support for newer Android versions.

P2P communication based on ISO/IEC 18092 is being discontinued and is no longer supported by NXP.

A similar situation applies when considering two PN5190 devices. Since P2P is no longer supported, the recommended approach would be to configure one PN5190 as the NFC reader and the second device in card emulation mode, rather than implementing a P2P configuration.

For new designs, we recommend using currently supported NFC operating modes and solutions.

 

Best regards

98 Views
Tinvs
Contributor I

Hello,

Thanks again, you have certainly steered us in the right direction. It is clear that P2P is not the way to go.

0 Kudos
Reply