Use LPC Debug NHS3100 DemoBoard debug Fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use LPC Debug NHS3100 DemoBoard debug Fail

2,465 Views
xiangxuejiao00
Contributor III

when I debug the app_demo_dp_tlogger demo project ,there are some errors happen like the picture in the attachment .

please tell me how to solve this problem ?

flash magic is OK to download the hex file .

if you need more information ,please let me know .

Version:  LPCXpresso v8.2.2 [Build 650] [2016-09-09] 

LPC-Link 2 Version: Rev B

NHS3100 SDK Version:release_mra2_11_2_nhs3100

Tags (1)
0 Kudos
Reply
1 Reply

2,354 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I tried with the same settings, but didn't meet your issue, please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply