Ucode I2C matching to 50 ohm ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ucode I2C matching to 50 ohm ?

2,550 Views
fletort
Contributor I

Hello,

i am really interesting by the Ucode I2C chip for tow reasons :

 - BAP feature

 - Interruption on Reader read operation.

But I am planning to use a 868Mhz ceramic chip already present on my board.

And, i don't know if a matching is available for this chip to match to 50ohm line ?

I found such a matching for another rfid chip from monza in one of their application note.

Is it possible with the ucode chip ?

0 Kudos
Reply
5 Replies

2,293 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Fabien,

I think you may refer to http://cache.nxp.com/documents/application_note/AN11180.pdf?fsrch=1&sr=4&pageNum=1  and http://cache.nxp.com/documents/application_note/AN11181.pdf?fsrch=1&sr=7&pageNum=1  for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,293 Views
fletort
Contributor I

thnaks i already read these documents. but no information are given for 50ohm matching.

0 Kudos
Reply

2,293 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Fabien,

Have you referred to http://www.nxp.com/documents/application_note/096917_UCODE_G2XM_G2XL_an.zip for details? Please note Ucode I2C impedance is 12.7-j199@915MHz, and this value should also be ok for 868MHz, but if you want to use  50ohm antenna , you have to use a 12.7+j199 to 50ohm Impedance transformation structure between the chip and antenna, for example , a Discrete L-Section Matching Network.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

849 Views
Shrfid
Contributor I

Hi NXP Team, 

 

the link http://www.nxp.com/documents/application_note/096917_UCODE_G2XM_G2XL_an.zip   is not available. 

 

Can you share the .brd file or the whole zip file with me? THX

0 Kudos
Reply

1,049 Views
Marcel_ArrowCE
Contributor II

Hi NXP Team, 

 

the link http://www.nxp.com/documents/application_note/096917_UCODE_G2XM_G2XL_an.zip   is not available. 

 

Can you share the .brd file or the whole zip file with me? THX
Marcel 

0 Kudos
Reply