Hi NXP :
After UPDATE_RF_CONFIG and LOAD_RF_CONFIG, that the value read from the Register 0x20 is different from the value set by UPDATE_RF_CONFIG, and only the Register address: 0x20 has this problem.
Setting log :
---Set RF configuration byte: 0x00, Register: 0x20--------------------------------------------------------------------
/*UPDATE_RF_CONFIG - RF configuration byte: 0x00, Register address: 0x20, Register value: 0x00DB8F22*/
Transmit: 12,00,20,22,8F,DB,00
Receive: -
---Read out to confirm -------------------------------------------------------------------------------------------------------------
/*RETRIEVE_RF_CONFIG_SIZE - RF configuration ID: 00*/
Transmit: 13,00
Receive: 08
/*RETRIEVE_RF_CONFIG - RF configuration ID: 00*/
Transmit: 14,00
Receive: 1,82,07,00,00,2F,02,00,00,00,16,50,23,00,00,42,04,01,24,00,14,10,00,00,0F,15,00,00,00,00,20,22,8F,DB,00,29,10,00,00,00 (successful)
---Load configuration--------------------------------------------------------------------------------------------------------------------------------
/*LOAD_RF_CONFIG - Transmitter configuration byte: 0x00, Receiver configuration byte: 0x80*/
Transmit: 11,00,80
Receive: -
---Read out from Register 0x20 to confirm ------------------------------------------------------------------------------------------------------------------
/*Read Register - Register address: 0x20*/
Transmit: 04,04,20
Receive: 01,4F,DB,00 (The Data is not my setting before)
Solved! Go to Solution.
Hi,
The sequence looks correct.
Please make sure that there is no other influence onto the register: Disable the AWC.
Regards,
Ivan.
Hi,
The sequence looks correct.
Please make sure that there is no other influence onto the register: Disable the AWC.
Regards,
Ivan.